Set PSK for mobile connectivity
Connect the supported
PowerFlex®
750-Series via Embedded
EtherNet/IP devices with the by setting a Pre-Shared Key (PSK)
and PSK ID and then deploying the security policy model.
IMPORTANT:
Follow standard password protection policies while
working with PSK and PSK IDs.
Prerequisites
- Ensure that you intend to configure a supported device for mobile connectivity. See Mobile connectivity.
- Deploy the security policy model to the device. See Deploy a policy model.
- To set PSK for mobile connectivity
- From the navigation bar, either:
- SelectCanvasand then select a device.
- SelectZonesand then select a zone and a device.
- SelectDevicesand then select a device.
- InPROPERTIES, underMobile connectivity, selectSet PSK.
- InSet Pre-Shared Key for mobile connectivity:
- Either generate or enter a unique Pre-Shared Key.TIP: PSK must include from 8 to 64 ASCII printable characters.
- Either generate or enter a unique Pre-Shared Key ID.TIP: PSK ID must include from 1 to 128 ASCII printable characters excluding commas.For example, enterPSK-mobile-001
- SelectSet PSK and PSK ID.
- Select either:
- Copy configuration. Copies the IP address, PSK and PSK ID into clipboard.
- Display QR code with configuration. Displays a QR code to scan with your mobile device. Once scanned, the IP address, PSK and PSK ID displays on the mobile device.IMPORTANT: Use a secure QR reader from a trusted vendor while working with PSK and PSK IDs.
- Enter the PSK and PSK ID into the .
Provide Feedback