Windows Firewall

Activate and configure the
Microsoft®
Windows firewall on a workstation to allow connections through the ports used to communicate with the AADvance or
Trusted®
controllers.
Configure other ports for the following scenarios:
  • Allow the workstations to access the Windows Updates, time synchronization, and anti-virus updates.
  • The Windows workstation may run additional software (such as HMI or data logging), therefore requiring the ports to pass through the firewall.
    TIP: Refer to the manufacturer’s manual for instructions about firewall settings.
Configure the firewall to allow these AADvance or
Trusted
system applications to communicate through the network:
Application Name
Application Description
AADOPCSV.exe
AADvance Gateway OPC DA Server
AADvDiscover.exe
AADvance Discover – Controller Discovery and Configuration
Wisaker.exe
Trusted
Simulator
ISaGRAF.exe
AADvance Simulator
tic_ver.exe
Trusted
TIC Version Checker
iniconfig.exe
Trusted
System Configuration Tool
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal