Network Firewall

When the network used by the AADvance or
Trusted®
system is connected to another network, the connections must pass through the firewall. These communication ports are supported by the
AADvance-Trusted SIS Workstation software®
:
Protocol
Port Number
Availability
Purpose
TCP
502
When configured
Modbus®
slave
TCP
1100
Used locally (remote access can be blocked)
Trusted Simulator
TCP
1132
Always available
AADvance, application downloads, debug, SOE, etc.
TCP
2000
When configured
Modbus RTU
TCP
6000
Always available
Trusted
, application downloads, debug, etc.
TCP
10001-10006
When configured (and the application is stopped)
Transparent Communications Interface (serial tunneling)
TCP
44818
Always available
CIP
produce and consume
TCP
55555
Always available
AADvance Diagnostic interface
TCP
23
Always available
Trusted Diagnostic interface
UDP
123
When configured
SNTP
UDP
1123, 1124
Always available
SNCP bindings
UDP
2010
Always available
Discovery and configuration protocol (DCP,
Rockwell Automation®
)
UDP
2222
When configured
CIP
produce and consume I/Os
UDP
5000
When at least one P2P subnet is active on a controller
Peer-to-Peer
UDP
44818
Always available
CIP
produce and consume
When the
Always available
ports are not configured or unused, they are open to unauthorized access. Perform the following actions to protect network ports:
  • If the network used by the system is connected to another network, the connection must pass through the firewall to protect the system from potential threats from other networks.
  • Configure the firewall to block all communication ports. If required, enable a specific port to a device needing to communicate with other devices on other networks.
  • The SNCP port must only be allowed to pass through the firewall if the
    Windows®
    PCs running the
    AADvance-Trusted SIS Workstation software
    are on a separate network.
  • The variable bindings port must only be allowed to pass through the firewall if the AADvance controller is communicating with another AADvance controller on a separate network.
  • The other communication ports (such as
    Modbus
    and SNTP), must only be allowed to pass through the firewall if the AADvance controller,
    Trusted
    controller, or
    Windows
    PC communicates with other devices on other networks.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal