Create an object from a type
Create an object from a type. The new object is automatically of the same type.
- FromType view, double-click the folder with the category of objects.
- Drag the desired object type and into a folder or object inProject view.
The new object appears in
Project view
with the name appended with (type)
.Provide Feedback