Create an OPC UA server for pushing UI objects

Create an OPC UA server that pushes the UI objects from the Server project and populates the Client project with them.
  1. In
    Project view
    , right-click the
    OPC-UA
    folder and select
    New
    OPC UA Server
    .
  2. In
    Properties
    , take a note of the
    Endpoint URL
    property value.
    NOTE: You need the
    Endpoint URL
    property value to configure the OPC UA Client later on.
  3. Next to
    Nodes to publish
    , select
    Add
    .
  4. Under
    Configuration1
    , set
    Publish dynamic configuration
    to
    True
    .
  5. Under
    Configuration1
    , next to
    Nodes
    , select
    Add
    .
  6. Under
    Nodes
    , create a dynamic link between
    Node1
    and
    ProjectName
    UI
    RemotePanels
  7. Under
    Configuration1
    , next to
    Nodes
    , select
    Add
    .
  8. Under
    Nodes
    , create a dynamic link between
    Node2
    and
    ProjectName
    Model
    .
  9. Next to
    Users
    , select
    Add
    .
  10. Set
    User1
    to
    Anonymous
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.