Integrate the module into a FactoryTalk environment with the FactoryTalk Directory
In this section, you will learn how to integrate a standalone
FactoryTalk Historian ME
module into an existing FactoryTalk system using the FactoryTalk Directory
. Integrating a standalone module into an existing FactoryTalk system allows:- Centralized administration of security credentials, performed in theFactoryTalk Administration Console.
- FactoryTalk clients (for example, FactoryTalk View SE or FactoryTalk Batch) to connect to theFactoryTalk Historian MEmodule.
Provide Feedback