Configure secure groups in the FactoryTalk Administration Console
To use the
FactoryTalk Directory
with FactoryTalk Historian ME
, you need to configure specific user groups in the FactoryTalk Administration Console
. If you have FactoryTalk Historian SE
installed in your environment, the secure groups should already exist in the FactoryTalk Administration Console
. Otherwise, you need to create them.There are the following secure user groups configured in the
FactoryTalk Administration Console
:- FTHAdministrators
- FTHEngineers
- FTHSupervisors
- FTHOperatorsIMPORTANT:If your user belongs to a different security group than the groups listed above, you will not be able to log on to theFactoryTalk Historian MEclient website. To manage your group access, contact the administrator.
If you plan to use the auditing features of
FactoryTalk Historian ME
while using FactoryTalk Security, you must create user IDs on the User Management
page that exactly matches the user IDs in the FactoryTalk Directory. This will allow you to track changes through a specific user and not a user group. An admin user who is a part of the FTHAdministrators group in the FactoryTalk Administration Console
must also belong to the FTHAdministrators, FTHSupervisors, and FTHEngineers groups on FactoryTalk Historian ME
. In addition, a user who belongs to the FTHEngineers group must also belong to the FTHSupervisors group to change events on FactoryTalk Historian ME
.Provide Feedback