Create users in the FactoryTalk Administration Console
You can add users to preconfigured user groups in the FactoryTalk Administration Console. Each user group is created automatically when the FactoryTalk Historian ME Management is installed. The FTHAdministrators, FTHEngineers, FTHOperators, and FTHSupervisors user groups represent different levels of user security. For details, see Understand privileges for user groups.
TIP:
For more information on FactoryTalk Security users and groups, see the
FactoryTalk Security User Guide
.To create a new FactoryTalk Historian ME user in the FactoryTalk Administration Console
- Go toStart > All Programs > Rockwell Software > FactoryTalk Administration Console.TheFactoryTalk Administration Consolewindow appears.
- In theSelect FactoryTalk Directorydialog box, clickNetwork, and then clickOK.TIP:FactoryTalk Historian ME and FactoryTalk Historian SE support only theNetworkoption in the FactoryTalk Directory.
- In theExplorerpane, expandUser and Groups.
- Right-clickUsers, and then clickNew > User.TheNew Userdialog box appears.
- Complete the user information.
- Click theGroup Membershiptab, and then clickAdd.TheSelect User Groupdialog box appears.
- Select the group to which you want the user to belong, and then clickOK.
- In theNew Userdialog box, clickOK.
- In theExplorerpane, expandUser Groups, and then double-click the group to which you added the new user.The new user is listed underMembers.
Provide Feedback