View archive data

To view archive data in FactoryTalk Historian ME, click the
View Data
tab, and then click
Archive Data
.
The page displays a list of points and the latest value collected for each point.
To view archive data
  1. Under
    Select Points For Archive Data
    , define your search criteria.
    For details, see Define search criteria.
  2. Click
    Search
    .
    The data is displayed in the
    Points
    table.
  3. Under
    Points
    , click a point for which you want to view data.
    TIP:
    You can view archive data only for one point at a time.
  4. In the
    Start Time
    and
    End Time
    boxes, type the start and end time for which you want to view the data.
    For details, see Set start and end times.
  5. Click
    View
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal