Set start and end times
The start and end times are set with relation to the time on the client computer.
The default start time is two minutes before the current time on the client computer. The default end time is the current time on the client computer.
You can use the following expressions to set time:
This expression | Means |
|---|---|
* | The current time. |
t | Today at midnight (00:00:00). |
y | Yesterday at midnight (00:00:00). |
t 15:00:00 | Today at 3:00:00 pm. |
y 15:00:00 | Yesterday at 3:00:00 pm. |
-60s | The past 60 seconds. |
+45m | The future 45 minutes. |
-5h | The past 5 hours. |
-3d | The past 3 days. |
sun | The most recent Sunday at midnight (00:00:00). |
25 8 | 08:00 on the 25th of the current month. |
25 8:10 | 08:10 on the 25th of the current month. |
06-dec-08 15:00:00 | 3:00:00 p.m. on December 6, 2008. |
mon+14.5h | 2:30:00 p.m. last Monday. |
sat-1m | 11:59:00 p.m. last Friday. |
Provide Feedback