FactoryTalk licensing
FactoryTalk Historian ME limits the clients that can access it. Client connections are limited to Rockwell Automation preferred clients. This means that no anonymous connections will be accepted. The following applications can access FactoryTalk Historian ME:
- FactoryTalk® Historian DataLink
- FactoryTalk®Historian ProcessBook
- FactoryTalk® View Site Edition (SE)Trending
- FactoryTalk® Administration Console
- PI System Management Tools (SMT)
- PI SMT Tag Configurator and PI Builder
- FactoryTalk® VantagePoint®and FactoryTalk VantagePoint EMI
Provide Feedback