Start and stop the data collection
TIP:
You must have administrator privileges to start and stop the data collection.
To start the data collection
- Click theConfigure Historiantab.TheData Collectionpage appears.
- ClickStart.
To stop the data collection
- Click theConfigure Historiantab.TheData Collectionpage appears.
- ClickStop.Make sure that that data collection is fully stopped before you start it again.TIP:You can also start and stop the data collection using:
- Controller programming languages (the Ladder logic).
- FactoryTalk Historian ME Logix Designer Module Profile.
For details, see Configure the module properties.
Provide Feedback