Collect data
The FactoryTalk Historian ME server collects data from the Logix controller through the chassis backplane. The data collection service then optionally performs a series of deadband tests on the data (exception and compression tests) and stores the data in the FactoryTalk Historian ME archive.
When started, the data collection service performs the following actions:
- Identifies all points listed as active, based on the value of theScanproperty in the points definition.
- Identifies (or registers) all controllers in the same Logix chassis by logical names, device IDs, and location (slot numbers).FactoryTalk Historian ME supports up to ten controllers. There is a maximum of five controllers in the local chassis and a maximum of five controllers in the remote chassis.
- Begins collecting data for all points based on the specified scan rate associated with each point.
Provide Feedback