Configure the module properties
Use the
Module Properties
dialog box to perform the following actions on your Historian module:- Restore the default settings.
- Reset the security configuration.
- Shut down the module.
- Start up the module.
- Refresh data about the module.
- Reset the module.TIP:Before you modify the module properties, back up your current module configuration.
To configure the module properties
- In RSLogix 5000 or Logix Designer, in the Controller Organizer, expandI/O Configuration.
- Right-click your Historian module, and then clickProperties.TheModule Propertiesdialog box appears.
- Click theConfigurationtab.TIP:The blue arrows next to the buttons indicate that the given action will be immediately committed, without pressing theApplybutton first.
- Choose any of the following options:
- Restore DefaultsClick this button to restore the module back to its original configuration.All configuration data, archives, and logs are deleted and reset.This process may take some time. While restoring the default settings, the Historian webpage will not be available.After you clickRestore Defaults, a message appears:ClickToYesPerform the restore defaults action.You will have 5 minutes to do either of the following:
- Cut off and restore the power to the module by turning off and on the power switch on the chassis.
- Unplug and insert the module into the chassis.
Otherwise, the action will be canceled.NoCancel the restore defaults action. - Reset SecurityResets the module security back to the FactoryTalk Historian ME Local Security mode and makes thepiadminuser the password empty.If the Historian module is in safe mode, clickingReset Securitywill have no effect. For details, see Repair archives using safe mode.After you clickReset Security, a message appears:ClickToYesPerform the reset security action.You will have 5 minutes to do either of the following:
- Cut off and restore the power to the module by turning off and on the power switch on the chassis.
- Unplug and insert the module to the chassis.
Otherwise, the action will be canceled.NoCancel the reset security action. - ShutdownShut down the module. This process may take some time.The module shutdown allows you to stop all FactoryTalk Historian ME related services (including the point server, the data collection, the data transfer, and the web configuration server). It is recommended that you shut down the module if you plan to remove it from the chassis or if you are going to power down the chassis.Before you perform any other operations in theConfigurationtab, wait until the shutdown is complete.
- StartupStart the module after it was shut down.When you click theStartupbutton, the module is rebooted, and the data collection service is restarted.The button is available only when the module is shut down.If Logix Designer Module Profile loses communication with the module at the startup time, the message "Requested message timed out" appears. ClickOKand retry.TIP:Alternatively, you can execute the Restore Defaults, Reset Security, and Shutdown actions using the FactoryTalk Historian ME web client.For details, see Restore and reset module-related settings, Reset the security mode, and Close and start the module.
- Click theModule Infotab.
- Choose any of the following options:
- RefreshClick this button to refresh the tab with new data from the module.
- Reset ModuleClick this button to reset the module.TIP:After restoring the module defaults configuration or resetting the security mode, change the password for the defaultadminuser.
Provide Feedback