Repair archives using safe mode

Each time you reboot the system, the system checks to see if your archive files contain any data that has a timestamp for a time in the future. If future timestamps are found upon rebooting, the module's STS light is solid red and the LED displays either
SAFE MODE LAN OK <IP_address>
or
SAFE MODE LAN LOST <MAC_address>
. Both messages indicate that the module is in safe mode. When this happens, the module web interface is inaccessible and you must go to the
Web Diagnostic
page to repair the archive files. When the module is in safe mode, PI commands cannot be executed.
When the module is in safe mode, the following error message appears on the
Web Diagnostics
page:
ERROR: Archives are in inaccessible state. Please navigate to "Safe Mode" or click on "Repair" to continue.
To access the bad archives information, follow the message instructions.
The bad archives are listed and selected by default.
You can repair the bad archives by repairing the time setting. For details, see Repair the time setting.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal