ChX view

Use the
ChX
view to configure a channel on 1756-OF4 and 1756-OF8 non-isolated analog output devices or configure an output channel on the 1756-IF4FXOF2F device.
Use the
ChX
view to:
  • Specify the output type and operating range
  • Specify the output state in Program Mode
  • Specify the output state in Fault Mode
  • If supported, enter scaling values
  • If supported, enter a sensor offset value
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal