Configure a channel
Create a channel-level configuration specific to your application.
To configure a channel on a non-isolated analog output device
- On the tab for the device, expandChannels, and then select an individual channel.
- In theChXview, customize the parameters as needed.
- SelectOKto save the changes.
Provide Feedback