Configure an output channel
Create a channel-level configuration specific to your application.
To configure an output channel on a high-speed analog I/O device
- On the tab for the device, expandOutput Channels, and then select an individual channel.
- In theChXview, customize the parameters as needed.
- SelectOKto save the changes.
Provide Feedback