AfterInputFieldUpload event
Occurs after one or all input field values are read. This occurs only once for an upload of all input fields.
Syntax
Display
_AfterInputFieldUpload
where
Display
– is the name of a Display object variable that was dimensioned using the WithEvents keyword or the reserved name Display.Provide Feedback