StringDisplay object

The StringDisplay object represents the intrinsic string display object. It is not a creatable object. StringDisplay objects are accessible through an Elements collection.
The object-specific properties for the StringDisplay object are merged with the Element object's properties. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Properties
Methods
Events
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal