NumericDisplay object

The NumericDisplay object represents the intrinsic numeric display object. It is not a creatable object. NumericDisplay objects are accessible through an Elements collection.
The object-specific properties for the NumericDisplay object are merged with the Element object's properties. This extended object is what you see when you directly access the object from VBA using the object's name.
Properties
Methods
Events
Constants
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal