Remove the delta value bar
When a delta value bar is not in use, you can remove the delta value bar.
To remove the delta value bar:
- At runtime, right-click the trend chart and then selectShow value bar.
Both the value bar and the delta value bar will be hidden from the chart. If you click
Show value bar
again, only the value bar will reappear on the trend chart.Provide Feedback