Use the delta value bar

Use the delta value bar to determine the difference between two x-axis points on a trend.
To use the delta value bar:
  1. At runtime, right-click the trend chart, select
    Active Value Bar > Delta
    .
  2. Click the trend chart at the first x-axis point to place the value bar.
  3. Click the trend chart at the second x-axis point to place the delta value bar.
The delta value bar indicates the difference between the two points.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal