Open trend properties from a button using the invoke command
If you are setting up only one or two buttons on your display, provide a button using the invoke command option on the
FactoryTalk View
display that opens trend property tabs.
TIP:
Operators can open the trend property tabs at runtime by right-clicking on the control and then selecting
Properties
.To open trend properties from a button using the invoke command
- Add a button to a graphic display, and then click theActiontab.
- Click the browse button next to theRelease Actionbox.
- In the right pane of the Command Wizard, clickInvoke, and then clickNext.
- From theDisplaylist, select the name of the graphic display where the trend is inserted.
- In theObjectbox, type the name of the trend (the default name is trend1).
- In theProperty or Methodbox, typeDisplayPropertyPages.
- ClickInvoke method in object.
- ClickFinish.
- ClickOKto close theButton Propertieswindow.
Provide Feedback