Find the object name of a trend object

When you insert a trend in a graphic display,
FactoryTalk View Studio
automatically assigns it a default object name of
trend1
. If you insert additional trends in the project,
FactoryTalk View Studio
increments the object name, like this: TrendX2, TrendX3, and so on.
To find the object name of a trend:
  • Right-click the control and then select
    Property Panel
    . Look for the
    (Name)
    property.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal