Open trend properties from a button using VBA

If you are setting up many buttons in your display, you can use the VBA option to help your application run faster.
To open trend properties from a button using VBA
  1. Add a button to a graphic display, and then click
    OK
    .
  2. Right-click the trend object and then select
    VBA code
    .
  3. Return to
    FactoryTalk View Studio
    , right-click the button object and then select
    VBA code
    .
  4. Type the name of the Trend object in the button released event code area.
    Private Sub Button1_Released()
    Trend1
    End Sub
  5. Press the period key and then select
    DisplayPropertyPages
    from the list.
    Trend1.DisplayPropertyPages
  6. Test the display.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal