Create a snapshot

Create a snapshot for an overlay.
TIP:
Settings on the
Runtime
tab control an operator's ability to create snapshots, and show or hide them at runtime.
To create a snapshot:
  1. Launch
    FactoryTalk View
    SE Client and run a trend graphic display.
  2. Right-click the runtime chart and then select
    Create Snapshot
    .
  3. In the
    Component Name box
    , type a name and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal