Edit shapes (TrendPro)

You can edit the shape to manually change it or add points to it.
To edit a shape
  1. Right-click the plot surface and select
    Shape > Edit
    .
  2. Use the cursor to drag the points (square boxes) on the shape to change the shape.
  3. Right-click the plot surface and click one of the following:
    • Add Point
      . Adds a point at the cursor's current location.
    • Undo
      . Removes a point.
    • Undo All
      . Removes all points that have been added using the
      Add point
      option.
    • Exit Edit
      . Exits edit mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal