Create new shapes (TrendPro)

When you create a shape that is not based on an existing trace, a rectangular shape displays on the plot surface and you can manually change the shape.
To create a new shape
  1. Right-click the plot surface and select
    Shape > New Default
    . A rectangular shape is added to the plot and you are placed in edit mode.
  2. Use the cursor to drag the square boxes on the corners of the shape to change the shape.
  3. Right-click the plot surface and select
    Exit Edit
    when finished.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal