About data servers

A data server provides a route to the physical devices on a network so you can access the values in those devices. For example, some of the values that data servers provide access to are:
  • programmable controller values.
  • OPC tags and their value or status information.
  • tags in a
    Studio 5000
    processor.
In
FactoryTalk View SE
the you can create:
  • a
    FactoryTalk Linx
    data server for use with
    FactoryTalk Linx
    that provides support for all products in the
    Studio 5000
    controller family including ControlLogix, CompactLogix, FlexLogix, DriveLogix, SoftLogix, and GuardLogix controllers, and other third-party controllers.
  • an OPC data server.
    An OPC data server can be used with RSLinx Classic to provide enhanced support for Rockwell Automation programmable controllers and devices. You can also use an OPC data server to provide support for any third-party data server that comply with the OPC DA 2.05a, UA 1.02 or 1.03 specifications.
  • a Tag Alarm and Event server for use with Alarm and Event graphic objects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal