Add a FactoryTalk Linx data server to an application
To access values in a ControlLogix controller, add a
FactoryTalk Linx
data server that will provide a link, in the form of direct references, between the application and the controller containing the tags that are being referenced.To add a
FactoryTalk Linx
data server:- In FactoryTalk View SE, in the Explorer window, right-click the application root or an area name, depending upon where you are adding the server, and then clickAdd New Server> Rockwell Automation Device Server (.FactoryTalk Linx)
- In thetabs, specify the required information for aFactoryTalk LinxServer PropertiesFactoryTalk Linxdata server.
- When finished, clickOK.
Remarks
- FactoryTalk Linxis optimized for use with all products in theStudio 5000controller family including ControlLogix, CompactLogix, FlexLogix, DriveLogix, SoftLogix, and GuardLogix controllers.
- When running a FactoryTalk View Site Edition application within a Windows workgroup, all Windows users should have Windows Administrative rights assigned to them.
- Names for the following FactoryTalk View Studio components do not support extended ASCII characters or Unicode characters: applications, areas, HMI servers, data servers, HMI tags,FactoryTalk Linxshortcuts, and FactoryTalk View Studio application files (. SED).
- For details adding and setting up aFactoryTalk Linxdata server, see theFactoryTalk LinxHelp.
Provide Feedback