Modify FactoryTalk Linx data server properties

Modify the properties of a
FactoryTalk Linx
data server to change settings for tag transfer and events.
To modify the
FactoryTalk Linx
data server properties:
  1. In the Explorer window, right-click the name of the
    FactoryTalk Linx
    data server, and then click
    Properties
    .
  2. In the
    FactoryTalk Linx
    Server Properties
    tabs, change the information as required, and then click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal