Set up data log file management
Use the
File Management
tab to specify when new files are created and old files are deleted. File Set
format files are created in sets of three. Data log files are named automatically by the system.To set up data log file management:
- In theData Log Modeleditor, click theFile Managementtab.
- If you are using theFile Setstorage format:
- In theStart New Filesarea, specify how to start new files when a particular event occurs.
- In theDelete Oldest Filesarea, specify how you want to delete old data log files if needed.
- If you are using theODBC databasestorage format, specify how you want to purge the oldest records in the ODBC database.
Provide Feedback