Data Log Models editor
How do I open the Data Log Models editor?
- InFactoryTalk View Studio, in theExplorerwindow, open theData Logfolder.
- Right-click theData Log Modelsicon, and then selectNew.TIP:You can also open theData Log Modelseditor by dragging its icon into the FactoryTalk View Studio workspace, or by double-clicking an existing Data Log Models component.
In the
Data Log Models
editor, you can create data log models that specify:- Which log file format to use.
- Where to store data log file sets (primary or secondary paths).
- When to create and delete log files.
- Which actions will trigger logging.
- Which tag values will be logged.
Provide Feedback