Turn on multiple language support in a graphic library

When you save the library display, all strings that can be switched are saved in the current application language. Only the text strings for the current language will be displayed. Text strings in any other language will appear as undefined strings. The strings will have to be translated before they will display in other languages.
To switch languages for the text strings in a graphic library, turn on multiple language support in the
Properties
tab of the
Display Settings
dialog box.
To turn on multiple language support in a graphic library:
  1. In the
    Graphics
    editor, open the
    Libraries
    folder.
  2. Right-click the graphic library, and then click
    Display Settings
    .
  3. In the
    Display Settings
    dialog box, in the
    Properties
    tab, select the
    Support Multiple Languages
    check box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal