Set up a client for language switching

In order to use language switching for an application or for a client, the first step is to install the languages and fonts that the application is to support. Install languages and fonts on your Windows operating system.
To set up a client for language switching:
  1. On the client computer, in your Windows operating system, install the languages and set up the fonts that the application is to support.
  2. When you create the
    FactoryTalk View SE
    configuration file, specify the initial language that the client is to open in.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal