Add a language to a FactoryTalk View SE application

Languages are added to an application using the Add button in the General tab of the Language Configuration dialog box. The list in the General tab shows the languages that have already been added to the application.
The list of languages that can be added to the application only shows languages supported by the operating system you are working in. If the language is listed, the fonts are properly installed. The languages that are installed by default vary depending on the operating system.
TIP:
  • The format for an RFC1766 identifier is:
    <languagecode2>-<country/regioncode2>
    where <languagecode2> is a lower case, two-letter code and <country/regioncode2> is an upper case, two-letter code. For example, the RFC1766 identifier for U.S. English is en-US.
  • Be sure the languages that an application is to support are installed on the development and client computers. If this is not done, the user might not be able to switch languages as expected. For example, if an application has been set up to switch between English and Chinese, but Chinese is not installed on the client machine, users might not be able to enter and display Chinese strings.
Prerequisites
  • Ensure the operating system supports the language
To add a language to a FactoryTalk View SE application
  1. In
    FactoryTalk View Studio
    , click
    Tools
    >
    Languages
    .
  2. In the
    Language Configuration
    dialog box, in the
    General
    tab, click
    Add
    .
  3. In the
    Add Language
    dialog box, select the language to be added to the application, and then click
    OK
    .
    The
    Add Language
    dialog box displays the name and RFC1766 identifier of each of the languages supported by the design-time computer. If the selected language is not installed, a warning message is displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal