Select a graphic display import or export operation

When you start the
Graphics Import Export Wizard
, the first thing you do is select the type of operation you are going to perform.
When you export graphic displays, an XML file with the same name as the display and the file extension .XML, is created for each display exported. In addition, a batch import file is created that is given the name
BatchImport_
<HMI Server name>
.XML
where
<HMI Server name>
is the name of the HMI server where the graphic display reside.
To select an operation type to perform:
  • Select
    Export graphic information from displays
    to export information about some or all of the graphic displays in the application in the form of XML text files. You can modify the XML files using Notepad, and then import the modified file into the application.
  • Select
    Import graphic information into displays
    to import one or more XML text files into the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal