Back up graphic displays before an import
When you select the import operation in the
Operation Type
dialog box in the Graphics Import Export Wizard
, the Backup
dialog box is opened. Here you decide whether or not to make backup copies of the files that will be overwritten when the selected files are imported.To back up the graphic display before an import:
- In theBackupdialog box, selectYesand clickNext. The dialog box that opens lets you specify a location for the backed up files.TIP:SelectNoto overwrite the files in the application where the files are being imported.
Provide Feedback