Select an export folder

Select the folder where you want the exported graphic XML files stored. By default, these are exported to the folder
My Documents
. To accept the backup location, click
Next
.
To select another folder to export files to:
  1. In the
    Export Folder
    dialog box, beside the
    Select the folder to export the graphic information to
    field, click the browse button
    (...)
    .
  2. In the
    Browse for Folder
    dialog box, specify a folder and click
    OK
    .
  3. In the
    Export Folder
    dialog box, click
    Finish
    . The selected graphic display files are exported to the folder as XML files.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal