Select a backup folder
Select the folder where you want the backup graphic files stored. By default, the application stores these files in the folder
My Documents
. To accept the backup location, click Next
.To select another backup folder:
- In theBackup Folderdialog box, beside theSelect the folder to backup the displays tofield, click the browse button(...). to open the .
- In theBrowse for Folderdialog box, specify the folder to backup the displays to and clickOK.
- In theBackup Folderdialog box, clickNext.The selected graphic display files are backed up to the selected location, and theImport File Typedialog box opens.
Provide Feedback