Set up version checking of stored displays
For clients to download ActiveX controls automatically when the display containing them is opened, you must set up the Internet Explorer options so that both unsigned and signed CAB files can be downloaded without prompt dialog boxes appearing each time.
To make sure that displays saved with a new version of an ActiveX control are sent to the SE Clients:
- In Internet Explorer, clickTools>Internet options.
- In theGeneraltab, clickSettingsin theTemporary Internet filesframe.
- In theSettingsdialog box, clickEvery visit to the page.
- ClickOKin theSettingsandInternet Optionsdialog boxes.TIP:In Internet Explorer if you leave the option Check for Newer versions of stored pages, set to Automatic, which is the default, Internet Explorer will not update the ActiveX control if a newer version exists.
Provide Feedback