Allow signed CAB files to download without prompts
For clients to download ActiveX controls automatically when the display containing them is opened, you must set up the Internet Explorer options so that both unsigned and signed CAB files can be downloaded without prompt dialog boxes appearing each time.
To allow signed CAB files to download from the Internet without prompts:
- In Internet Explorer, clickTools>Internet options.
- In theSecuritytab, clickInternetfor the zone.
- ClickCustom Levelto set the security level for the zone.
- In theSecurity Settingsdialog box, in theReset custom settingsframe, selectMediumin theReset tofield.
- ClickResetandOKin theSecurity Settingsdialog box.
- ClickOKin theInternet Optionsdialog box.
Provide Feedback