Run an SE client

Use the
FactoryTalk View SE
Client Wizard to run the client configuration file to verify the behavior of the configuration file before distributing it to workstations.
To run a client file:
  1. On the home page of the
    FactoryTalk View SE
    Client Wizard, click
    Run a client file
    .
  2. On the
    Select client file
    page, do one of the following:
    • Select a file name from the list of recent client files.
    • Click the browse button to select a file name and then click
      Run
      .
    • Type the full path name and then click
      Run
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal