Test an application
When developing an application, you can test that components work as you intend them to. To do this, use the to create a SE client that will connect to the application you are developing and start the components you want to test.
FactoryTalk View
SE Client WizardTo test run an application
- InFactoryTalk View Studio, selectTools>Launch SE Client.
- In theFactoryTalk ViewSE Client Wizard, clickCreate a, and follow the on-screen instructions.FactoryTalk View SEClient configuration file
- When complete, clickRun. The graphic display you specified to run initially will open in the FactoryTalk View SE Client window.
Provide Feedback