Create a graphic display

Use the Graphics editor to create a graphic display, and then add a graphic object to that display.
To create a display
  • In the
    FactoryTalk View
    Explorer window, expand the HMI server and the Graphics folder, right-click
    Displays
    and select
    New
    .
To add a graphic object to the display
  1. In the Toolbox, select an object. For example,
    Drawing
    >
    Rectangle
    .
  2. Drag the mouse to draw the approximate size that the rectangle is to be.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal