Import a project for an HMI server - network station
When you import a project, you can use an RSView32 project, a
FactoryTalk View ME
project, or an HMI project from a FactoryTalk View SE
application.
TIP:
For more information about importing a FactoryTalk View ME project, see Knowledgebase Document ID: QA601 - FactoryTalk View ME to FactoryTalk View SE Conversion.
To import a project for an HMI server:
- InFactoryTalk View SE, in the Explorer window, right-click the application root or right-click an area name, depending upon where you are adding the server, and then clickAdd New Server > HMI Server.
- In theSelect Operationwindow of theHMI Server wizard, clickImport a project > Next.
- In theImport Projectwindow, in theProject typefield, click down arrow to display the types of projects that can be imported, and then click one to select it.
- Beside theProject filefield, click theBrowse (...)to browse for the project files that are available.
- In theOpendialog box, double-click a project, and then click the project's .sed file >Open.This copies the path and name of the SED file into theImport Projectwindow.
- ClickNext.
- In theNew HMI Server Propertieswindow, type a name and description for the new HMI server.
- Type or browse for the name of the computer that will host the new HMI server and then clickFinish.
Provide Feedback