Upload
In a graphic display, reads a value from the programmable controller or OPC server and displays it in the selected numeric input objects.
This command is run on the currently active display on the
FactoryTalk View SE
Client or FactoryTalk View Studio
that issued the command. It will be ignored when it is issued from an HMI Server or if no display is active.Provide Feedback