DownloadAll
Writes the values in all the input fields in the active graphic display to the programmable controller or OPC server.
This command is run on the currently active display on the
FactoryTalk View SE
Client or FactoryTalk View Studio
that issued the command. It will be ignored when it is issued from an HMI Server or if no display is active.Provide Feedback