Download

Writes the value in the selected input field in the active graphic display, to the programmable controller, or OPC server.
You can also press Enter to download the value in the selected input field. If you use the /E parameter with the Display command to open the graphic, the Enter key is not available and you will have to use the Download command.
This command is run on the currently active display on the
FactoryTalk View SE
Client or
FactoryTalk View Studio
that issued the command. It will be ignored when it is issued from an HMI Server or if no display is active.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal